2022-05-27 1:40 PM
Hi, it seems to be a common error in STM32 devices. It happens when I try to validate on target after analyze the model. I tried to fix it according to the answers in community. But those solutions given in community or other websites doesn't help. At least for my board they doesn't help.
Infomation:
The device: STM32H735G-DK
MCU: STM32H735IGK6
CubeMX 6.5.0 with X Cube AI v7.1.0, v7.0.0 & v 6.0.0
Model: The model given in official tutorial of X-cube-ai.
CN15 STLK √
JP7: CHGR/USBFS
SW1: Set to 1
USART3 Enabled: PD8 & PD9
Baud Rate: 115200
Word Length:8 bit
No Parity
Stop bits: 1
ST-Link connectivity works normally. (Able to connect with CubeProgrammer).
It can be built in Keil and could be load to the board, with LD6 blinking in red and green. I am looking forward to solutions to this problem.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.