2026-02-19 7:38 AM
I installed the latest STM32Cube AI Studio along with STM32CubeMX 6.16.0, STM32CubeProgrammer 2.21.0, and ST Edge AI Core.
CubeMX has STM32CubeU5 Firmware Package V1.8.0 / 04-June-2025 installed.
All attempts to run a neural network end with:
../../Middlewares/ST/AI/Misc/Inc/ai_device_adaptor.h:624:8: error: unknown type name 'UART_HandleTypeDef'
When AI Studio generates a project from any neural network, it disables the UART in stm32u5xx_hal_conf.h.
Even if I uncomment the #define of HAL_UART_MODULE_ENABLED, the app cannot be compiled because the stm32u5xx_hal_uart.h header was never generated.
If I click on the little gear at the upper right in Cube AI Studio, it shows me that the COM5 LPUART1 is configured.
So I'm stuck -- Cube AI Studio cannot be used with the stm32u5xx devices.
Any advice?
Thanks!
--Mike
Solved! Go to Solution.
2026-02-19 9:12 AM
I reproduced the issue, it seems that STM32Cube AI Studio was not able to find the default VCP for this board. Also, the GUI shows values where they are only shown because they are "first" in the array.
Could you please try the following:
- Open your project in STM32Cube AI Studio
- Change the pins in the parameters to the following:
- UART interface: USART1
- RX PIN: PA10
- TX PIN: PA9
We will fix this issue in the next release.
Best regards,
Yanis
2026-02-19 8:30 AM
Hello,
Could you please share what is the MCU / Board you are working with?
Could you also share logs you had during the execution?
You can retrieve the logs in C:\users\<username>\.stm32cubeaistudio\logs
Best regards,
Yanis
2026-02-19 8:47 AM
2026-02-19 9:12 AM
I reproduced the issue, it seems that STM32Cube AI Studio was not able to find the default VCP for this board. Also, the GUI shows values where they are only shown because they are "first" in the array.
Could you please try the following:
- Open your project in STM32Cube AI Studio
- Change the pins in the parameters to the following:
- UART interface: USART1
- RX PIN: PA10
- TX PIN: PA9
We will fix this issue in the next release.
Best regards,
Yanis
2026-02-19 9:46 AM
Thank you, Yanis!
That solved it.
--Mike
2026-02-19 11:58 PM
Good news!
Have a good day.
Yanis
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.