2025-07-24 7:00 PM
[INFO] : Quantization complete.
[INFO] : Evaluating the quantized model using validation_set...
INFO: Created TensorFlow Lite XNNPACK delegate for CPU.
100%|██████████| 36/36 [05:01<00:00, 8.37s/it]
[INFO] : Accuracy of quantized model on validation_set = 98.17%
[INFO] : Evaluation complete.
[INFO] : Using the local download of STM32Cube.AI. Link to download https://www.st.com/en/embedded-software/x-cube-ai.html
[INFO] : Starting the model memory footprints estimation...
[WARN] : STM32Cube.AI installed version 2.1.0 does not match the version specified in user_config.yaml file 10.1.0 !
[INFO] : STM32Cube.AI version 2.1.0 used.
Error executing job with overrides: []
Traceback (most recent call last):
File "C:\st\stm32ai-modelzoo-services-main\.venv\lib\site-packages\clearml\binding\hydra_bind.py", line 230, in _patched_task_function
return task_function(a_config, *a_args, **a_kwargs)
File "C:\st\stm32ai-modelzoo-services-main\image_classification\stm32ai_main.py", line 399, in main
process_mode(mode=mode, configs=cfg, train_ds=train_ds, valid_ds=valid_ds, quantization_ds=quantization_ds,
File "C:\st\stm32ai-modelzoo-services-main\image_classification\stm32ai_main.py", line 315, in process_mode
chain_tqeb(cfg=configs, train_ds=train_ds, valid_ds=valid_ds, quantization_ds=quantization_ds, test_ds=test_ds)
File "C:\st\stm32ai-modelzoo-services-main\image_classification\stm32ai_main.py", line 233, in chain_tqeb
benchmark(cfg=cfg, model_path_to_benchmark=quantized_model_path, credentials=credentials)
File "C:\st\stm32ai-modelzoo-services-main\common\benchmarking\common_benchmark.py", line 58, in benchmark
_stm32ai_benchmark(footprints_on_target=board,
File "C:\st\stm32ai-modelzoo-services-main\common\benchmarking\common_benchmark.py", line 549, in _stm32ai_benchmark
_analyze_footprints(offline=offline, results=cloud_res, stm32ai_output=stm32ai_output, inference_res=inference_res, target_mcu=target_mcu)
File "C:\st\stm32ai-modelzoo-services-main\common\benchmarking\common_benchmark.py", line 80, in _analyze_footprints
with open(os.path.join(stm32ai_output, 'network_report.json'), 'r') as f:
FileNotFoundError: [Errno 2] No such file or directory: 'C:\\st\\stm32ai-modelzoo-services-main\\image_classification\\src\\experiments_outputs\\2025_07_25_09_01_04/stm32ai_files\\network_report.json'
Set the environment variable HYDRA_FULL_ERROR=1 for a complete stack trace.
进程已结束,退出代码为 1
Solved! Go to Solution.
2025-07-25 1:47 AM
I think I have solved this problem. I just need to replace the X-CUBE-AI version with 10.0.0
2025-07-24 7:08 PM
network_report.json file have not been created!
2025-07-24 11:41 PM
i append some log in common_benchmark.py.
# Run generate command locally
command = f"{path_to_stm32ai} generate --target stm32 -m {model_path} -v 0 --output {stm32ai_output} --workspace {stm32ai_output} --optimization {optimization}"
# command = f"{path_to_stm32ai} generate --target stm32n6 -m {model_path} --st-neural-art user_neuralart.json"
print("command00 = {}".format(command))
args = shlex.split(command, posix="win" not in sys.platform)
print("command01 = {}".format(command))
subprocess.run(args, env=new_env, check=True)
print("command02 = {}".format(command))
except subprocess.CalledProcessError as e:
raise TypeError(
f"Received: stm32ai.path_to_stm32ai={path_to_stm32ai}. Please specify a correct path to STM32Cube.AI!") from e
return stm32ai_output
[INFO] : STM32Cube.AI version 2.1.0 used.
command00 = C:/Users/Administrator/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/10.1.0/Utilities/windows/stedgeai.exe generate --target stm32 -m ./pretrained_models/best_model.h5 -v 0 --output C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\src\experiments_outputs\2025_07_25_14_33_22/stm32ai_files --workspace C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\src\experiments_outputs\2025_07_25_14_33_22/stm32ai_files --optimization balanced
command01 = C:/Users/Administrator/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/10.1.0/Utilities/windows/stedgeai.exe generate --target stm32 -m ./pretrained_models/best_model.h5 -v 0 --output C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\src\experiments_outputs\2025_07_25_14_33_22/stm32ai_files --workspace C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\src\experiments_outputs\2025_07_25_14_33_22/stm32ai_files --optimization balanced
command02 = C:/Users/Administrator/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/10.1.0/Utilities/windows/stedgeai.exe generate --target stm32 -m ./pretrained_models/best_model.h5 -v 0 --output C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\src\experiments_outputs\2025_07_25_14_33_22/stm32ai_files --workspace C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\src\experiments_outputs\2025_07_25_14_33_22/stm32ai_files --optimization balanced
Error executing job with overrides: []
Traceback (most recent call last):
File "C:\st\stm32ai-modelzoo-services-main\.venv\lib\site-packages\clearml\binding\hydra_bind.py", line 230, in _patched_task_function
return task_function(a_config, *a_args, **a_kwargs)
File "C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\stm32ai_main.py", line 399, in main
process_mode(mode=mode, configs=cfg, train_ds=train_ds, valid_ds=valid_ds, quantization_ds=quantization_ds,
File "C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\image_classification\stm32ai_main.py", line 309, in process_mode
benchmark(cfg=configs)
File "C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\common\benchmarking\common_benchmark.py", line 58, in benchmark
_stm32ai_benchmark(footprints_on_target=board,
File "C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\common\benchmarking\common_benchmark.py", line 551, in _stm32ai_benchmark
_analyze_footprints(offline=offline, results=cloud_res, stm32ai_output=stm32ai_output, inference_res=inference_res, target_mcu=target_mcu)
File "C:\st\stm32ai-modelzoo-services-main_bak\stm32ai-modelzoo-services-main\common\benchmarking\common_benchmark.py", line 80, in _analyze_footprints
with open(os.path.join(stm32ai_output, 'network_report.json'), 'r') as f:
FileNotFoundError: [Errno 2] No such file or directory: 'C:\\st\\stm32ai-modelzoo-services-main_bak\\stm32ai-modelzoo-services-main\\image_classification\\src\\experiments_outputs\\2025_07_25_14_33_22/stm32ai_files\\network_report.json'
Set the environment variable HYDRA_FULL_ERROR=1 for a complete stack trace.
2025-07-25 12:42 AM
Hello @fanronghua0123456,
Can you share the yaml you used? And the model if possible?
Else, do you see this issue with other models?
Have a good day,
Julian
2025-07-25 1:04 AM
2025-07-25 1:47 AM
I think I have solved this problem. I just need to replace the X-CUBE-AI version with 10.0.0
2025-07-25 6:04 AM
Hello @fanronghua0123456,
Yes, it seems that you don't have the version 2.1.0 installed on your pc.
For now I would suggest sticking to the 10.0.0 version for testing. But if you can, please use the last version available as each version fixes bugs.
Have a good day,
Julian
2025-07-27 5:45 PM
Julian,
Thanks for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.