2024-03-14 6:17 AM
I have a LSTM model which was quantized using TensorFlowLite full integer quantization. After that, I wanted to try deploy the model on the SensorTile Box. I tried analyzing the model but it throws the following error:
[AI:network] NOT IMPLEMENTED: UNIDIRECTIONAL_SEQUENCE_LSTM with output type (SIGNED, 8 bit, C Size: 8 bits Scales: [0.007843137718737125] Zeros: [-1] Quantizer: UNIFORM) not supported
I would be really grateful for ideas or insights on how to solve this!
2024-03-14 10:39 AM
Hi Fare,
With the 8.1, the fully quantized version (int8) of the UNIDIRECTIONAL_SEQUENCE_LSTM operator is not supported. It will be supported in the new X-CUBE-AI release with the cell_state in 16b as converted by TFLite converter.
br
jm
2024-03-15 2:21 AM
Hello Jean,
Thank you for your reply. I found out that in X-CUBE-AI on CubeMX, it provides two different runtime, TFLite Micro and STM32Cube.AI. When I try to analyze it with the TFLite Micro runtime, I am able to analyze the model. Does that mean that this runtime supports the UNIDIRECTIONAL_SEQUENCE_LSTM operator?
What's the difference between these two runtimes?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.