2019-09-13 10:44 AM
I have a problem with STM32; when i connect my FC the STM32 it isn't detected from my pc, it doesn't appear in device manager. What is the problem? I have windows 10 a OS. I tried out to install cube programmer, zadig, but STM32 isn't detected. Thanks for the support!!
2019-09-13 10:53 AM
What board are you using ?
If you are using an ST board with an embedded ST-Link make sure you connect the board on the USB port marked ST-Link.
Also, you may download the STLink firmware upgrade to upgrade the firmware on the ST-Link https://www.st.com/en/development-tools/stsw-link007.html
and the driver https://www.st.com/en/development-tools/stsw-link009.html
Regards
Daniel
2019-09-13 11:04 AM
Some Flight Controller? Be SPECIFIC, perhaps cite a web page for the specific hardware you're talking about.
Device might not be powered correctly
Device might not be in the correct mode to connect. Is there a BOOT button, are you connecting via USB?
Does ANYTHING show up in Device Manager? What?
Try a different cable
Try a different port
Avoid docking stations and hubs
2019-09-13 11:18 AM
Sorry, i am using a SP Racing F3 as flight controller, and on it is installed the STM32. The whole thing is to manage a x220 wizard.
I tried out to change port, usb cable, also with boot button, but when i connect it to pc in device manager, in particular in "USB devices", there isn't STM32. Thanks for the answers.I attached the manual about the FC.I tried on modeling sites but nobody can give me answers and I think it's a problem with the STM32.
2019-09-13 11:25 AM
According to the documentation you need an external standalone ST-Link to program and debug the embedded MCU
https://www.st.com/en/development-tools/st-link-v2.html
2019-09-13 12:08 PM
So i have to buy this module? Can't be solved by installing some special software?
2019-09-13 12:10 PM
Thanks for the suggestion, is there any other help? Because other that are bought this drone haven't bought this module, this is why it seems strange to me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.