2025-05-15 8:25 AM
Hi,
When changing from a Tiny YOLOv2 model to ST SSD Mobilenet v1 I strangely got the following error:
Bus interface interrupt
BUSIF0 ERR: 0x10
BUSIF1 ERR: 0x0
ATON_STD_IRQHandler()@763: irqs=0xlx
assertion "0" failed: file "Y:/VM/stm-workspace/fall-guard-v2.0.0/Lib/AI_Runtime/Npu/ll_aton/ll_aton_runtime.c", line 767, function: __LL_ATON_RT_IrqErr
I tried other models but only Mobilenet v1 always returns this error. Is there a specific config required?
Thanks,
Gino
Solved! Go to Solution.
2025-05-27 4:47 AM - edited 2025-05-27 5:23 AM
Hello
Thanks for the input, and the tests you did.
Thanks also for the full project.
Thanks.
2025-05-27 6:28 AM
Hi @Creator,
I successfully ran st_ssd_mobilenet_v1_025_192_int8.tflite on the people detection project. Please find attached the patch allowing for such support.
Steps:
Note: make sure to use the last stedgeai release (v2.1).
Guillaume
2025-05-27 12:18 PM
Hi @GRATT.2 ,
With this latest version of people dettection project I was also able to run my model and am able to detect a fall.
I've uploaded a working version here: https://www.swisstransfer.com/d/5a548741-4d5a-43eb-9cf1-b3fc665dd493
I am still not sure what went wrong in my project because I kind of did everyting that was stated in the patch file. This version of people detect had extra buffer definitions
#define NN_OUT_NB 3
#define NN_OUT0_SIZE (6825 * 3 * 4)
#define NN_OUT1_SIZE (6825 * 4 * 4)
#define NN_OUT2_SIZE (6825 * 4 * 4)
==> Can this be related?
Thanks for the solution, from this point I can continue my fall detection project.
Grts,
Gino
2025-05-30 5:51 AM
Hi, @GRATT.2 , @Julian E. , @SlothGrill ,
Since the people detection project V2.0.0 is based on freertos and the nxduo library is not compatible with freertos, I've looked further into the bug.
The root cause seemed to be in the nn_thread_fct function and how the output buffer is managed.
Now I have a working version using threadx of my project. It's updated on github: ginodecock/fall-guard-od: Detect a fall by using object detection using the stm32n6570-dk board
Can you guys check within ST that the people detection project V1.0.0 also can get this fix?
Thanks,
Gino
2025-06-03 7:01 AM
Hello @Creator,
A patch was published in the last version of the people detection project V2.0.0 that should fix.
Have a good day,
Julian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.