2023-12-17 9:29 PM
When designing stm32 AI, the values come out, but the learned values don't seem to come out. This is training data using 12 variables. Please help me if there is a problem with the code.
/* System headers */
#include <stdint.h>
#include <stdlib.h>
#include <stdio.h>
#include <inttypes.h>
#include <string.h>
#include "app_x-cube-ai.h"
#include "main.h"
#include "ai_datatypes_defines.h"
#include "network.h"
#include "network_data.h"
/* USER CODE BEGIN includes */
/* USER CODE END includes */
/* IO buffers ----------------------------------------------------------------*/
#if !defined(AI_NETWORK_INPUTS_IN_ACTIVATIONS)
AI_ALIGNED(4) ai_i8 data_in_1[AI_NETWORK_IN_1_SIZE_BYTES];
ai_i8* data_ins[AI_NETWORK_IN_NUM] = {
data_in_1
};
#else
ai_float* data_ins[AI_NETWORK_IN_1_SIZE_BYTES] ;
#endif
#if !defined(AI_NETWORK_OUTPUTS_IN_ACTIVATIONS)
AI_ALIGNED(4) ai_i8 data_out_1[AI_NETWORK_OUT_1_SIZE_BYTES];
ai_i8* data_outs[AI_NETWORK_OUT_NUM] = {
data_out_1
};
#else
ai_float* data_outs[AI_NETWORK_OUT_1_SIZE_BYTES];
#endif
/* Activations buffers -------------------------------------------------------*/
AI_ALIGNED(32)
static uint8_t POOL_0_RAM[AI_NETWORK_DATA_ACTIVATION_1_SIZE];
ai_handle data_activations0[] = {POOL_0_RAM};
/* AI objects ----------------------------------------------------------------*/
static ai_handle network = AI_HANDLE_NULL;
static ai_buffer* ai_input;
static ai_buffer* ai_output;
static void ai_log_err(const ai_error err, const char *fct)
{
/* USER CODE BEGIN log */
if (fct)
printf("TEMPLATE - Error (%s) - type=0x%02x code=0x%02x\r\n", fct,
err.type, err.code);
else
printf("TEMPLATE - Error - type=0x%02x code=0x%02x\r\n", err.type, err.code);
do {} while (1);
/* USER CODE END log */
}
static int ai_boostrap(ai_handle *act_addr)
{
ai_error err;
/* Create and initialize an instance of the model */
err = ai_network_create_and_init(&network, act_addr, NULL);
if (err.type != AI_ERROR_NONE) {
ai_log_err(err, "ai_network_create_and_init");
return -1;
}
ai_input = ai_network_inputs_get(network, NULL);
ai_output = ai_network_outputs_get(network, NULL);
#if defined(AI_NETWORK_INPUTS_IN_ACTIVATIONS)
/* In the case where "--allocate-inputs" option is used, memory buffer can be
* used from the activations buffer. This is not mandatory.
*/
for (int idx=0; idx < AI_NETWORK_IN_NUM; idx++) {
data_ins[idx] = ai_input[idx].data;
printf("1");
}
#else
for (int idx=0; idx < AI_NETWORK_IN_NUM; idx++) {
ai_input[idx].data = data_ins[idx];
printf("2");
}
#endif
#if defined(AI_NETWORK_OUTPUTS_IN_ACTIVATIONS)
/* In the case where "--allocate-outputs" option is used, memory buffer can be
* used from the activations buffer. This is no mandatory.
*/
for (int idx=0; idx < AI_NETWORK_OUT_NUM; idx++) {
data_outs[idx] = ai_output[idx].data;
}
#else
for (int idx=0; idx < AI_NETWORK_OUT_NUM; idx++) {
ai_output[idx].data = data_outs[idx];
}
#endif
return 0;
}
static int ai_run(ai_float *in_data, ai_float *out_data)
{
ai_i32 batch;
ai_input[0].data = AI_HANDLE_PTR(in_data);
ai_output[0].data = AI_HANDLE_PTR(out_data);
batch = ai_network_run(network, &ai_input[0], &ai_output[0]);
if (batch != 1) {
ai_log_err(ai_network_get_error(network),
"ai_network_run");
return -1;
}
// out_data[0] = ((ai_float *) (ai_output[0].data))[0];
return 0;
}
/* USER CODE BEGIN 2 */
int acquire_and_process_data(ai_i8* data[])
{
/* fill the inputs of the c-model
for (int idx=0; idx < AI_NETWORK_IN_NUM; idx++ )
{
data[idx] = ....
}
*/
return 0;
}
int post_process(ai_float* data[])
{
/* process the predictions
for (int idx=0; idx < AI_NETWORK_OUT_NUM; idx++ )
{
data[idx] = ....
}
*/
((ai_float *)data)[0] = (ai_float)1.0f;
((ai_float *)data)[1] = (ai_float)5.0f;
((ai_float *)data)[2] = (ai_float)1.0f;
((ai_float *)data)[3] = (ai_float)1.0f;
((ai_float *)data)[4] = (ai_float)1.0f;
((ai_float *)data)[5] = (ai_float)1.0f;
((ai_float *)data)[6] = (ai_float)1.0f;
((ai_float *)data)[7] = (ai_float)1.0f;
((ai_float *)data)[8] = (ai_float)1.0f;
((ai_float *)data)[9] = (ai_float)1.0f;
((ai_float *)data)[10] = (ai_float)1.0f;
((ai_float *)data)[11] = (ai_float)1.0f;
return 0;
}
/* USER CODE END 2 */
/* Entry points --------------------------------------------------------------*/
void MX_X_CUBE_AI_Init(void)
{
/* USER CODE BEGIN 5 */
ai_boostrap(data_activations0);
/* USER CODE END 5 */
}
void MX_X_CUBE_AI_Process(void)
{
float y_val;
/* USER CODE BEGIN 6 */
post_process(data_ins);
ai_run(data_ins,data_outs);
for(int i=0;i<12;i++)
{
printf("%f\r\n",((float *)data_ins)[i]);
}
y_val = ((float *)data_outs)[0];
printf("output: %f\r\n",y_val);
HAL_Delay(1000);
/* USER CODE END 6 */
}
#ifdef __cplusplus
}
#endif
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.