2022-03-15 3:08 AM
Is it needed to do the learning on every device? Or can the library be used on all devices of the same class?
Solved! Go to Solution.
2022-03-15 3:10 AM
It is possible to use the same library (both static and dynamic) on all devices of the same class. The following scenario is possible: prepare representative HW/SW setup then learn the dynamic model (Anomaly Detection), backup the knowledge and clone the knowledge to every device (working under similar conditions), please see :
2022-03-15 3:10 AM
It is possible to use the same library (both static and dynamic) on all devices of the same class. The following scenario is possible: prepare representative HW/SW setup then learn the dynamic model (Anomaly Detection), backup the knowledge and clone the knowledge to every device (working under similar conditions), please see :
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.