2025-06-23 10:50 AM
Hi,
I am currently working with the nucleo-n657x0-q and trying to validate a tflite model on it. While it works in the neural-ART runtime I cant seem to get a validation program working for the MCU runtime. For the neural-ART runtime I followed the NPU_Validation guide from the 2.1 ST Edge projects package, this worked without problem.
For the MCU runtime, my first approach was to follow the guide mentioned above but omit the --st-neural-art flag for the ST cli generate command, when running the n6_loader.py script this results in a "Compilation failed". Attached are the logs produced with the error.
My second approach was to use the cubeMX to generate a validation program. The main issue here is that each time that I enable validation in the X-cube-ai package the software freezes 99% of the time. I have been able to work around this issue by first creating a template program in MX and then changing to validation and regenerating the code. What I am stuck on now is that I do not know how to proceed with the program. Using validation on host in the .ioc only results in the following errors:
E200(ValidationError): TARGET: Unable to bind the ST.AI runtime with "network" c-model: [] E801(HwIOError): could not open port 'COM3': PermissionError(13, 'Access is denied.', None, 5)
Why am I getting these errors and is there a different approach that I am missing? Attached is also the MX generated project.
Thanks in advance,
Brian.
Solved! Go to Solution.
2025-06-26 1:01 AM - edited 2025-06-26 6:51 AM
Hello @brianon,
So, I learned that it is indeed not currently supported.
It will be added in the next update, ST Edge AI Core 2.2.
I don't have the exact date, but it should come out in around 2 weeks.
Have a good day,
Julian
2025-06-25 8:08 AM
Hello @brianon,
Thank you for the information, I will try to replicate.
Have a good day,
Julian
2025-06-26 1:01 AM - edited 2025-06-26 6:51 AM
Hello @brianon,
So, I learned that it is indeed not currently supported.
It will be added in the next update, ST Edge AI Core 2.2.
I don't have the exact date, but it should come out in around 2 weeks.
Have a good day,
Julian
2025-06-26 8:59 AM
Hi @Julian E.,
That is unfortunate. For clarities sake, does this extend to all x-cube-ai functionality on the MCU runtime for the stm32n6 board or is it only validation that is not yet supported?
2025-06-27 12:11 AM
Hello @brianon,
To my knowledge, it is only the validation that is not yet supported.
Have a good day,
Julian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.