2019-10-28 6:26 AM
Hy everyone,
is possible to configure different values for MLC_ODR, FSM_ODR, XL_ODR and GYRO_ODR, or they must be set equals each others?
Thanks and best regards,
Leonardo M.
2019-10-31 2:49 AM
Hi Leonardo, it is possible to set different ODRs, but it is recommended to set the same ODR for MLC output, gyro and axl, or at least the same for the input data of axl and gyro. The chosen ODR depends on the activity you want to classify: in case of gym activity, for example, the recommended ODR will be higher (e.g. 104Hz) then in case of motion intensity (12.5Hz recommended). Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.