2024-08-29 10:05 PM
Hi All,
I’m trying to hunt down the best board for my new project. Basically I need the following functionality either on the board or via add-on boards. I can see a few possibilities but I haven’t had much experience so I thought it best to ask. Thankyou!
Requirements
Not a requirement but would be great
2024-10-08 3:05 AM - edited 2024-10-09 12:02 AM
Hello @mzvitzf ,
Sorry for the late reply.
Seeing your requirements, all I can think of is the u85 IoT: B-U585I-IOT02A - Discovery kit for IoT node with STM32U5 series - STMicroelectronics
But it has not ethernet port and not the right audio codex.
This board is what we use for all AI audio event sound detection use case, so it is compatible with model zoo deployment for audio event detection use case as well. You can take a look here: https://github.com/STMicroelectronics/stm32ai-modelzoo/tree/main/audio_event_detection/deployment
You can also take a look at the STM32U575I-EV but it is somewhat pricy and does not have a RJ45, a audio out and is not low power...
Have a good day,
Julian
2025-06-01 1:17 AM
What a great query! A few standout microprocessor boards for TinyML/AI projects with an emphasis on audio are: The Arduino Nano 33 BLE Sense is small and has a built-in microphone, making it ideal for finding keywords and easy audio classification. With TinyML libraries like TensorFlow Lite for Microcontrollers, the Raspberry Pi Pico with an external microphone is both affordable and adaptable. Seeed XIAO ESP32S3 Sense – The ESP32's AI capabilities, small form factor, and onboard microphone make it an excellent choice for low-power audio tasks. The Syntiant NDP101/120 is ideal for always-on voice interfaces and is designed specifically for ultra-low power audio AI at the edge. Your power budget, model complexity, and use case (voice commands versus ambient sound classification, for example) all play a role.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.