2023-09-25 12:30 PM
Hello,
how can I reset FIFO_Get_Rotation_Vector in LSM6DSV16x sensor?
Regards,
Fehmi.
Solved! Go to Solution.
2023-09-27 5:49 AM
Ciao @FKara.3 ,
Can you write me the register name and the bit you are referring to?
Thanks
2023-09-27 5:49 AM
Ciao @FKara.3 ,
Can you write me the register name and the bit you are referring to?
Thanks
2023-09-28 7:54 PM
Ciao @Federica Bossi ,
/*
@file LSM6DSV16X_Sensor_Fusion.ino
@author STMicroelectronics
@brief Example to use the LSM6DSV16X library with Sensor Fusion Low Power.
*******************************************************************************
Copyright (c) 2022, STMicroelectronics
All rights reserved.
This software component is licensed by ST under BSD 3-Clause license,
the "License"; You may not use this file except in compliance with the
License. You may obtain a copy of the License at:
opensource.org/licenses/BSD-3-Clause
*******************************************************************************
*/
#include <LSM6DSV16XSensor.h>
#define ALGO_FREQ 120U /* Algorithm frequency 120Hz */
#define ALGO_PERIOD (1000U / ALGO_FREQ) /* Algorithm period [ms] */
unsigned long startTime, elapsedTime;
LSM6DSV16XSensor AccGyr(&Wire);
uint8_t status = 0;
uint8_t tag = 0;
float quaternions[4]={0};
void setup() {
Serial.begin(115200);
while (!Serial) yield();
Wire.begin();
// Initialize LSM6DSV16X.
AccGyr.begin();
// Enable Sensor Fusion
status |= AccGyr.Enable_Rotation_Vector();
if(status != LSM6DSV16X_OK) {
Serial.println("LSM6DSV16X Sensor failed to init/configure");
while(1);
}
Serial.println("LSM6DSV16X SFLP Demo");
}
void loop() {
uint16_t fifo_samples;
// Get start time of loop cycle
startTime = millis();
// Check the number of samples inside FIFO
if(AccGyr.FIFO_Get_Num_Samples(&fifo_samples) != LSM6DSV16X_OK){
Serial.println("LSM6DSV16X Sensor failed to get number of samples inside FIFO");
while(1);
}
// Read the FIFO if there is one stored sample
if (fifo_samples > 0) {
for (int i = 0; i < fifo_samples; i++) {
AccGyr.FIFO_Get_Tag(&tag);
if(tag==0x13u){
AccGyr.FIFO_Get_Rotation_Vector(&quaternions[0]);
// Print Quaternion data
Serial.print("Quaternion: ");
Serial.print(quaternions[3], 4);
Serial.print(", ");
Serial.print(-quaternions[1], 4);
Serial.print(", ");
Serial.print(quaternions[0], 4);
Serial.print(", ");
Serial.println(quaternions[2], 4);
// Compute the elapsed time within loop cycle and wait
elapsedTime = millis() - startTime;
delay(ALGO_PERIOD - elapsedTime);
}
}
}
}
Previously, I was reading quaternion values from FIFO but now I can't because fifo_samples shows 0.
Regards,
Fehmi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.