2025-09-25 12:42 AM
https://community.st.com/t5/stm32-mcus/how-to-build-an-ai-application-from-scratch-on-the-nucleo-n657x0/ta-p/828502
There was a problem while following this guide.
In dev mode, the signed binary files are programmed in cubeprogrammer and re-run in flash mode, and the blue light remains on. (The FSBL main() runs normally)
I set BOOT_Application() to breakpoint through CUBEIDE and debugged line by line.
An error occurred in img_size = BOOT_GetApplicationSize(uint32_t) source for CopyApplication
source:<error: Cannot access memory at address 0x70100000>
destination:<error: Cannot access memory at address 0x24050000>
I have confirmed that there is an error.
0x70100000 I programmed the signed application file in that area
What is the reason for this problem?
2025-09-25 5:37 AM
destination address should be 0x34000000 as that is where the secure RAM block starts so try setting destination address to this inside cube mx
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.