2023-05-26 12:25 AM
I want to know when will stm cube ai support keras 2.12.0 because for now it only support up till 2.11.0. I can't seem to downgrade my keras version as it require to downgrade more dependencies.
Furthermore I converted my lstm keras (h5) model to tflite but it gives me "transpose of batch size not supported" error on analyze any solution?
2023-05-26 1:02 AM
Support for TF/Keras 2.12 has been introduced in X-CUBE-AI 8.1 that will be available mid june.
I'm interested to have your tflite network that you can't import to see if it is supported now or if I should open a bug to the development team.
Regards
2023-05-26 2:29 AM
2023-05-26 2:41 AM
There is already a bug opened on this issue with a similar model, I've added yours and let you know when it is fixed
2023-05-26 2:46 AM
Ok np, I will wait for the next version. one more question in this model i have used the batch size of 32 should i decrease the batch size to 1 and re-analyze?
2023-06-21 3:45 AM
hi i am facing the same error
how i can i fix the issue ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.