2025-02-28 6:56 AM
Hello,
I am encountering an issue when converting a TensorFlow Dense layer to .tflite and subsequently using the ST Edge AI tool to convert it to .nb format, following the ST Edge AI Guide for MPU.
When using a lower-dimensional input, the conversion succeeds. For example, the following code works as expected:
input_features = tf.keras.Input(shape=(1, 384), dtype=tf.float32)
output = tf.keras.layers.Dense(1536)(input_features)
model = tf.keras.Model(inputs=input_features, outputs=output)
However, increasing the input dimension to (1500, 384) results in the following error:
ST Edge AI Core v2.0.0-20049
PASS: 0%| | 0/2 [00:00<?, ?it/s]
Galcore warning: MMU is disabled!
E [main.c:vnn_VerifyGraph:93]CHECK STATUS(-3:The requested set of parameters produce a configuration that cannot be supported.)
E [main.c:main:236]CHECK STATUS(-3:The requested set of parameters produce a configuration that cannot be supported.)
E 21:37:15 Fatal model generation error: 64768
E010(InvalidModelError): Error during NBG compilation, model is not supported
Is there a known limitation on the input/output dimensions for Dense layers when converting to .nb format? If so, is there a recommended approach to handle larger dimensions, or any workarounds to enable successful conversion and NPU acceleration?
Thank you for your time and assistance.
Best regards,
Justin
Solved! Go to Solution.
2025-03-03 2:35 AM
Hello @J-WTY ,
You can find the constraint regarding the ST Edge AI Core here: https://stedgeai-dc.st.com/assets/embedded-docs/index.html
Depending on what you use, meaning tensorflow, tflite, keras or onnx and if you use the NPU (example: STM32N6), the constraint on the layers may be different. You can find a dedicated page for each one of them.
There is a commun constraint that is this one:
(None,)) is considered as equal to 1[0, 65536[NHWC format)
So, instead of using a (1500,384) shape, please use a (1,1500,384) shape. For example:
input_features = tf.keras.Input(shape=(1, 1500, 384), dtype=tf.float32)
output = tf.keras.layers.Dense(1536)(input_features)
model = tf.keras.Model(inputs=input_features, outputs=output)
2025-03-03 2:35 AM
Hello @J-WTY ,
You can find the constraint regarding the ST Edge AI Core here: https://stedgeai-dc.st.com/assets/embedded-docs/index.html
Depending on what you use, meaning tensorflow, tflite, keras or onnx and if you use the NPU (example: STM32N6), the constraint on the layers may be different. You can find a dedicated page for each one of them.
There is a commun constraint that is this one:
(None,)) is considered as equal to 1[0, 65536[NHWC format)
So, instead of using a (1500,384) shape, please use a (1,1500,384) shape. For example:
input_features = tf.keras.Input(shape=(1, 1500, 384), dtype=tf.float32)
output = tf.keras.layers.Dense(1536)(input_features)
model = tf.keras.Model(inputs=input_features, outputs=output)
2025-03-18 9:09 AM
Hello Julian E.,
Thanks for your answer, I'm sorry for ignoring your reply for days.
with the help of your suggestion, I will try to solve it as soon as possible, thanks!
Best regards,
J-WTY
2025-03-23 6:09 PM
Hello @Julian E.
I found it work to use (1, 1500, 384) for the shape of Input layer!
Thanks for your help a lot!
But I want to know that is this due to the constraint "1D operator is mapped on the respective 2D operator by adding a singleton dimension on the input: (12,3) -> (12, 0, 3)"? Thanks!
Best regards,
J-WTY
2025-03-24 7:00 AM
Hello @J-WTY,
Thanks for the update!
Regarding your question, I am not exactly sure.
In my opinion, because ST Edge AI core was originally made for images, they probably already had 2D operators in C code.
So instead of developing the 1D variant for each operator, they mapped your 1D input to 2D as it is probably the same thing either way.
Keep in mind that I am speculating here, but I think it is a reasonable explanation.
Have a good day,
Julian
2025-03-29 2:05 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.