2022-10-03 11:06 PM
2022-10-03 11:43 PM
Since the Machine Learning Core in LSM6DSOX supports only decision trees as machine learning models, Unico-GUI generates only decision trees as classifier for this device.
However, considering that the MLC in LSM6DSOX can run up to eight different decision trees in parallel, generating outputs in different registers (MLC0_SRC, MLC1_SRC, MLC2_SRC, etc), it is possible to read the outputs of the different trees and try to combine the results in a custom way at MCU level.
The sensor itself is able to run the decision trees in parallel and the user can decide which decision tree has to generate an interrupt through the MLC_INT1 / MLC_INT2 registers.
2022-10-03 11:43 PM
Since the Machine Learning Core in LSM6DSOX supports only decision trees as machine learning models, Unico-GUI generates only decision trees as classifier for this device.
However, considering that the MLC in LSM6DSOX can run up to eight different decision trees in parallel, generating outputs in different registers (MLC0_SRC, MLC1_SRC, MLC2_SRC, etc), it is possible to read the outputs of the different trees and try to combine the results in a custom way at MCU level.
The sensor itself is able to run the decision trees in parallel and the user can decide which decision tree has to generate an interrupt through the MLC_INT1 / MLC_INT2 registers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.