2020-07-07 7:00 PM
[webinar - Program decision trees in sensors with a Machine Learning Core]
Solved! Go to Solution.
2020-07-07 7:03 PM
The Machine Learning Core (MLC) configuration has to be created with the Unico GUI, since it contains all the specific hardware settings of the ST devices. Unico GUI can also run offline, in order to create a configuration even without any ST development board connected to the PC.
Once the device configuration has been created with Unico (.ucf or .h file), it can be flashed on ST sensors featuring the MLC capability as shown by the example available on the ST GitHub repository.
2020-07-07 7:03 PM
The Machine Learning Core (MLC) configuration has to be created with the Unico GUI, since it contains all the specific hardware settings of the ST devices. Unico GUI can also run offline, in order to create a configuration even without any ST development board connected to the PC.
Once the device configuration has been created with Unico (.ucf or .h file), it can be flashed on ST sensors featuring the MLC capability as shown by the example available on the ST GitHub repository.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.