2016-02-23 4:47 AM
I got a freescale motherboard compatible with the SPC56EL70L5. With it, I got the PE universal multilinker (USB-ML-UNIVERSAL), and I'd like to use it instead of SPC5-UDESTK with UDE to connect to the SPC56EL70L5. Do you know if it possible or not? What kind of target configuration?
Thank you very much2016-02-23 5:26 AM
Hello Stefano ,
PE universal multilinker is not supported by UDE.For this, i would use S32 Design Studio available on Freescale/NXP website.there are some PE Micro Debug Feature. 1) GNU E200 PEMicro Interface Debugging Support 1.1.6.201511041643 com.pemicro.debug.gdbjtag.ppc.feature.feature.group PEMicro Microcomputer Systems 2) C/C++ GDB Hardware Debugging 8.6.0.201502131403 org.eclipse.cdt.debug.gdbjtag.feature.group Eclipse CDTon eclipse point of view, you can reintegrate it in SPC5Studio andtake the launch configuration given by S32 Design Studio.
Best Regards ErwanWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.