2023-10-25 12:29 PM
Hi,
I'm currently working with a discovery board SPC58EC-DISP and I´m using a SPC5-UDESTK for debug, my issue is the next:
The first 2 - 3 days the UDE STK 5.2 works properly, I can connect to the board without problem, but after those days I am not able to connect with the board, it shows the next message
I delete and installed again the UDE STK 5.2 and I was able to connect to the board again but after few days Im facing the same issue, I have two laptops and in both Im facing the same issue, also the power supply and all the configuration is the same when it connects to the board and when it doesn´t connects, I read in some forums that it could be a power supply issue but definitely this is not the case because nothing changes when it works and when not..
also Im not the only one with this issue:
https://community.st.com/t5/microcontrollers/problems-with-ude-visual-platform/td-p/468544
Can you please help me?
Regards,
Elio Zepeda
Solved! Go to Solution.
2025-09-04 5:11 PM
Hi Ethan,
I didn’t solve the issue, but I found that uninstalling and reinstalling the debugger driver temporarily fixes the problem.
The driver installation executable can be found under:
C:\Program Files\pls\UDE Starterkit 2021\Driver\JtagUsbDriver
2023-10-26 7:25 AM
Hello ,
could you try 64 bits version Download SPC5-UDESTK (pls-mc.com) ?
I recommend to contact PLS
Best regards
Erwan
2023-11-07 9:42 AM
@Erwan YVIN Why is your answer set as accepted solution if the issue is not resolved and if I don´t even prove your suggested solution?, I will try installing that version and I will let you know if that works.
Regarding to contact PLS this was their answer:
Dear valued Partner,
Thank you for interest in SPC5/UDESTK.
The SPC5/UDESTK is a product of STM which is based on PLS’s technology. The support for this special product is provided by STM, only.
Please get support from here:
http://www.st.com/web/en/support/support.html
Limitation in comparison to the full featured professional PLS tools are:
Regarding the issue:
The error message tell that nothing has been detected at JTAG.
Reason might be:
Best regards
Your PLS SPC5-UDESTK team
2024-03-04 12:27 AM
Hi eliozepeda,
I was wondering if you managed to solve this issue later on. How did you resolve it?
Thanks,
Best regards,
Ethan
2025-09-04 5:11 PM
Hi Ethan,
I didn’t solve the issue, but I found that uninstalling and reinstalling the debugger driver temporarily fixes the problem.
The driver installation executable can be found under:
C:\Program Files\pls\UDE Starterkit 2021\Driver\JtagUsbDriver
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.