2018-08-19 8:45 PM
SPC5 Studio for SPC560D-DIS board, LINFLEX0 configured as UART, Tx is okay but Rx ISR is not getting called. I am using the auto generated Serial Test application which creates IRQ handlers in "spc5_linflex.c". I have break points set in both Tx and Rx IRQ handlers, only Tx IRQ gets hit. I can see the RX data coming into BDRM buffer and UARTSR DRF (data receive flag) is also set. Please help.
2018-08-29 1:47 AM
Hello,
are you using spc5studio 5.8.1?
If not please update your version of SPC5Studio to 5.8.1 and let us know if the problem still exist.
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.