2018-08-27 3:02 AM
Hello,
I've got a problem with max analog channel input voltage. When all supply voltages are 5V everything is fine. But if VDD_HV_IO_MAIN voltage is 3.3V while VDD_HV_ADV is 5V, the analog channel input voltage becomes limited over 4V. This problem is observed both on my PCB and on the EVB (SPC57xxMB + SPC58XXADPT176S REV. B). Can you help me resolve the problem?
2018-08-28 12:17 AM
More test results for the problem: MCU temperature increases for 6-7 degrees. It seems the analog channel internal circuit scheme protection is referenced by VDD_HV_IO_MAIN (instead VDD_HV_ADV). Сan someone clarify this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.