2018-02-05 5:39 AM
Hi ,
I'm new and I 'm developing on SPC570S40E1.
I've a demo board and my final target board.
When I try to debug my application I've 2 different behavior between demo board and final target:
on demo board during clock initialization I see by ME_GS register that the system is DRUN mode, while , on my final target, sw go in irqSysHalt called by spc_clock_init SPC5_CLOCK_FAILURE_HOOK because system mode is RUN0.
My demo board is SPC570S-DISP , my target is the same micro 64 pin and I use UDESTK with microUSB.
On the final target , after load the program, if I power on the board, the program run correctly, while with Debugger don't run because is locked in irqSysHalt.
#spc570s40e1 #ude #udestk2018-02-06 2:35 AM
Hello Guglielmo ,
No problem is noticed on
SPC570S-DISP.
Could you check the application SPC570Sxx_RLA SERIAL Test Application for Discovery located in SPC5Studio ?
Did you use the same way of debugging (PLS) for your final board ?
Best regards
Erwan
2018-02-07 2:59 AM
Hello Erwan,
Yes, on final board I'm using SPC5-UDESTK PLS USB/JTAG adapter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.