2021-09-21 3:43 AM
We have just ran the update for SPC5 and on regenerating the application we get this message. What can we do to solve that?
/Larsa
Solved! Go to Solution.
2021-09-22 1:46 AM
Hello,
the customization (in driver source files) are memorized in a project file "patch.xml" (available in the root directory of the project).
Every time that the User re-generate the code, the customization are applied to the source files.
This message is reported when the patches are no more necessary (patch code is already present in the source file) or when totally not aligned with the source file.
If, it is in the second case, please apply the patch manually, ignoring the SPC5Studio message.
BR,
Emanuele
2021-09-22 1:46 AM
Hello,
the customization (in driver source files) are memorized in a project file "patch.xml" (available in the root directory of the project).
Every time that the User re-generate the code, the customization are applied to the source files.
This message is reported when the patches are no more necessary (patch code is already present in the source file) or when totally not aligned with the source file.
If, it is in the second case, please apply the patch manually, ignoring the SPC5Studio message.
BR,
Emanuele
2021-09-22 2:19 AM
That makes sense, thanks Emanuele!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.