2014-09-23 6:46 AM
I am using UDE 4.2.05 with the SPC560B-DIS (which has UDE debug hardware built in)
I can load and run code via JTAG but ... How do I access the serial port connection to the target device ??? The target microcontroller UART is connected to the FTDI USB/serial/JTAG device but I do not see a COM port show up on the PC for the target USB/serial connection. Should this show up as a COM port or perhaps in a UDE window ??Solved! Go to Solution.
2014-09-24 1:59 AM
Hello Adams ,
you can find in attachment a document how to install the driver : Best regards Erwan ________________ Attachments : FTDI_Installation_driver_on_SPC560X_Discovery_board_cx369645_1.0_D2.docx : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Sb&d=%2Fa%2F0X0000000bZB%2FGShbxE0szlE8Amb7z3DQ1Ritv2kaXV0g8YUUrwBAm1E&asPdf=false2014-09-23 8:01 AM
2014-09-24 1:59 AM
Hello Adams ,
you can find in attachment a document how to install the driver : Best regards Erwan ________________ Attachments : FTDI_Installation_driver_on_SPC560X_Discovery_board_cx369645_1.0_D2.docx : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Sb&d=%2Fa%2F0X0000000bZB%2FGShbxE0szlE8Amb7z3DQ1Ritv2kaXV0g8YUUrwBAm1E&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.