2024-09-20 12:56 AM
Hello,
I currently have SPC560P chip which I am able to program using SPC5 Studio and Debug using SPC5-UDESTK. The compiler that I have currently selected is "FreeGCC with VLE Support" by going to the Application Configuration -> SPC560Pxx Platform Component RLA -> Build Settings.
I see the other options in the dropdown of Compiler Variant such as Hightech and GreenHills.
The issue that I am currently facing is that I am modifying only a part of the existing code and I need to use another compiler when merging with the old code. So I was wondering if I can change the compiler to "mwcceppc" from "FreeGCC with VLE Support" in SPC5 Studio ? If Yes, how ?
I have added the path to "mwcceppc" in the SPC5 Studio -> Windows -> Preferences -> C/C++ -> Build -> Environment. And also the same in Project Properties. But I believe the settings in Configuration.xml will override these settings ?
Let me know if this is a possibility or not.
Solved! Go to Solution.
2024-09-24 12:42 AM
Hello ,
yes , it is possible to use CDT in Makefile mode (not Makefile generated) in order to add to your own compiler.
Maybe , you need to create your C project (CDT) and import the configuration in your CDT Project.
Best Regards
Erwan
2024-09-24 12:42 AM
Hello ,
yes , it is possible to use CDT in Makefile mode (not Makefile generated) in order to add to your own compiler.
Maybe , you need to create your C project (CDT) and import the configuration in your CDT Project.
Best Regards
Erwan
2024-09-24 1:05 AM
Correct me if I am wrong, In the case suggested by you, I will import my existing project and use my own Makefile and this will be a standalone project in SPC5 Studio. I will not be able to use PinMap Editor or Configuration.xml file correct as it is not a SPC5 C/C++ Application ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.