2018-09-04 3:49 PM
Good morning
We connected the board spc570 by microUSB, our operating system (both windows 7 and windows 10) detected it as "SPC570S-DISP discovery board" but can't install any driver. We have already downloaded and installed SPC5 studio with "complete installation" but it seems that it can't be aware of the connected device: we can generate application code and compile a test application but we can't execute and debug it because execute and debug button remains always grayed. So we will ask if we have to buy something else or we have to download some specific driver or change some setting on the PC.
best reguard
2018-09-06 12:47 AM
Hello ,
it is not SPC5Studio .. it is linked to PLS UDE
PLS JTAG is integrated in your board
Could you check with PLS UDE 4.10 ?
https://www.pls-mc.com/login-a-384.html?User=SPC5UDESTKUser
You have to install it
Best regards
Erwan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.