cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5 reset mode sets pin to high

PNeub.2
Associate II

I'm using the SPC5EC58 chip, and i want to switch some relays. This works so far. The problem is, during the reset mode even i'm setting it by Hardware like by a button or in the debugging mode, the pins which controlls the relays are set to high, can i somehow disable that ? because the board is used in a critical environment, where the relays shouldn't be triggered by something like the reset.

0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.