cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with running application on SR6G7

andreih
Associate

Hello,

I am trying to run Projects\System\SIUL2\siul2LedBlink from StellarSDK_4.0.0 on a SR6G7EVBC4000P_RevA board. The project was successfully build. 

To flash the board in RAM, I am using the last version of Lauterbach. When running, it seems that it can't break on main.

For testing purposes, I was running the sieve_ram_aarch32_arm_v8r_le.elf using the same Lauterbach script and the execution and breaking on main was done as expected. On a deeper investigation, I have found out that the .elf file form Lauterbach differs from the one build. Those differences can be seen below.

elf_comparison.png

Also, I have tried running an example from Lauterbach using the NVM, but I get the following error: 

image.png

 

Do you have any suggestions to run Projects\System\SIUL2\siul2LedBlink on the board? Also, to flash an application on NVM and fix the flash programming error.

 

Thanks in advance :grinning_face:

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
FSPIL
ST Employee

Hello Andrei,

SR6 information is provided under NDA.
For any question, please contact local ST support, and do not post information/questions in this public forum.

Thank you.

 

Best regards,

Francesco


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Erwan YVIN
ST Employee

Hello , 

I am checking with Local FAE and SDK SR6

                         Best regards

                                     Erwan

 

              

FSPIL
ST Employee

Hello Andrei,

SR6 information is provided under NDA.
For any question, please contact local ST support, and do not post information/questions in this public forum.

Thank you.

 

Best regards,

Francesco


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.