2019-06-03 8:45 AM
We use SPC560P50L5 in an automotive-qualified battery management system for starter batteries. PIT timer of this device should be able to generate a wake-up interrupt when in low-power mode.
At this moment, PIT timer 3 is already working to generate an interrupt at the end of a certain time period. The user manual states that it is possible to use the PIT timer to leave low-power mode (STOP0). But it is unclear which registers are used for that, and how we have to configure them.
NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.
Solved! Go to Solution.
2019-06-03 8:46 AM
For PIT to be used for wake-up it needs some additional settings, so let me summarize following three main points:
1. CLK has to be enabled for PIT, but since PIT3 is already working I suppose that this point is done
- Register PITMCR_MDIS
2. Interrupt has to be enabled and you have to clear the flag after an interrupt has occured.
- Register TCTRL3 for enable
- Register TFLG3_TIF for clearing flag
3. Configure the STOP0 mode to keep the PIT enabled and working
- ME_STOP0_MC for configuration of used mode, important is that SYSCLK is running.
- ME_LP_PC0_STOP0 should be enabled.
- ME_PCTL92_LP_CFG should be set to “000�?, which selects ME_LP_PC0 configuration.
2019-06-03 8:46 AM
For PIT to be used for wake-up it needs some additional settings, so let me summarize following three main points:
1. CLK has to be enabled for PIT, but since PIT3 is already working I suppose that this point is done
- Register PITMCR_MDIS
2. Interrupt has to be enabled and you have to clear the flag after an interrupt has occured.
- Register TCTRL3 for enable
- Register TFLG3_TIF for clearing flag
3. Configure the STOP0 mode to keep the PIT enabled and working
- ME_STOP0_MC for configuration of used mode, important is that SYSCLK is running.
- ME_LP_PC0_STOP0 should be enabled.
- ME_PCTL92_LP_CFG should be set to “000�?, which selects ME_LP_PC0 configuration.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.