2015-06-16 11:40 PM
Hello,
I am a newer of SPC studio, while I am learning SPCstudio, I read help docs such as ''SPC560Pxx OS-less OSAL Component User Manual.chm'' I don't understand how this function ''osalThreadSleepMilliseconds(1000);'' implement ,even though I go into it for details. Does anyone know how this function works? It sleeps for a while ,then wake up,or it use a system timer (STM) to delay some time. Thanks! #spcstudio2015-06-17 1:26 AM
osalThreadSleepMilliseconds(1000); is based system tick calculated from the PIT Channel 0
(Periodic Interrupt Timer) (cf below)/**
* @brief PIT channel 0 interrupt handler.
*
* @isr
*/
OSAL_IRQ_HANDLER(vector59) {
OSAL_IRQ_PROLOGUE();
osalSysLockFromISR();
osalOsTimerHandlerI();
osalSysUnlockFromISR();
/* Resets the PIT channel 0 IRQ flag.*/
PIT.CH[0].TFLG.R = 1;
OSAL_IRQ_EPILOGUE();
}
Initilialization is done in hal_lld_init()
/* PIT channel 0 initialization for Kernel ticks, the PIT is configured
to run in DRUN,RUN0...RUN3 and HALT0 modes, the clock is gated in other
modes.*/
INTC.PSR[59].R = SPC5_PIT0_IRQ_PRIORITY;
halSPCSetPeripheralClockMode(92,
SPC5_ME_PCTL_RUN(2) | SPC5_ME_PCTL_LP(2));
reg = halSPCGetSystemClock() / OSAL_ST_FREQUENCY - 1;
PIT.PITMCR.R = 1;
/* PIT clock enabled, stop while debugging. */
PIT.CH[0].LDVAL.R = reg;
PIT.CH[0].CVAL.R = reg;
PIT.CH[0].TFLG.R = 1;
/* Interrupt flag cleared. */
PIT.CH[0].TCTRL.R = 3;
/* Timer active, interrupt enabled. */
Best Regards
Erwan
2015-06-17 8:53 PM
hi, erwan!
Thank you so much! I will go trough it.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.