2016-02-26 12:53 AM
Hello,
I have read the core manual of SPC56EL70 (e200z4). I want to handle the IVOR1 exception with an interrupt routine in configuration.xml in SPC5Studio. It's not clear to me what I should write in the ISR in question (what number? IVOR1 is not present in INTC chapter in the reference manual)Thank you very much2016-02-26 1:55 AM
2016-02-26 2:18 AM
I'm talking about the first one.
So:I can just write an assembly routine, and I have to add at some point (I don't know exactly) of ivor.s:#if CORE_SUPPORTS_DECREMENTER /* * _IVOR1 */ .align 4 .globl _IVOR1 .type _IVOR1, @function_IVOR1: /* Creation of the external stack frame (extctx structure).*/ stwu %sp, -80(%sp) /* Size of the extctx structure.*/#if PPC_USE_VLE && CORE_SUPPORTS_VLE_MULTI e_stmvsrrw 8(%sp) /* Saves PC, MSR. */ e_stmvsprw 16(%sp) /* Saves CR, LR, CTR, XER. */ e_stmvgprw 32(%sp) /* Saves GPR0, GPR3...GPR12. */#else /* !(PPC_USE_VLE && CORE_SUPPORTS_VLE_MULTI) */ stw %r0, 32(%sp) /* Saves GPR0. */ mfSRR0 %r0 stw %r0, 8(%sp) /* Saves PC. */ mfSRR1 %r0 stw %r0, 12(%sp) /* Saves MSR. */ mfCR %r0 stw %r0, 16(%sp) /* Saves CR. */ mfLR %r0 stw %r0, 20(%sp) /* Saves LR. */ mfCTR %r0 stw %r0, 24(%sp) /* Saves CTR. */ mfXER %r0 stw %r0, 28(%sp) /* Saves XER. */ stw %r3, 36(%sp) /* Saves GPR3...GPR12. */ stw %r4, 40(%sp) stw %r5, 44(%sp) stw %r6, 48(%sp) stw %r7, 52(%sp) stw %r8, 56(%sp) stw %r9, 60(%sp) stw %r10, 64(%sp) stw %r11, 68(%sp) stw %r12, 72(%sp)#endif /* !(PPC_USE_VLE && CORE_SUPPORTS_VLE_MULTI) *//*routine execution */ b _ivor_exit#endif /* CORE_SUPPORTS_DECREMENTER */Do I miss something?2016-03-01 5:28 AM
2016-03-01 5:49 AM
That's something I'm struggling with: I need it in order to handle uncorrectable errors. I must disable ECSM reporting because I don't want a reset on DED in my application, but I don't have any mechanism to inject a DED avoiding reset: even if I enable ECSM reporting just for the injection, as the error is injected with
SPP_MCM.EEGR.R= 0x0220; //uncomment these three lines to inject uncorrectable error 0x00014008: 70 1F E7 F4 E_LIS R0,0xFFF4 0x0001400C: 70 E0 02 20 E_LI R7,0x220 0x00014010: 01 06 SE_MR R6,R0 0x00014012: 5C E6 00 4A E_STH R7,0x4A(R6)*((uint32_t *) 0x40002000) = PATTERN; 0x00014016: 62 10 SE_BGENI R0,0x1 0x00014018: 65 20 SE_BSETI R0,0x12 0x0001401A: 70 EA E5 55 E_LIS R7,0x5555 0x0001401E: 70 EA C5 55 E_OR2I R7,0x5555 0x00014022: 01 06 SE_MR R6,R0 0x00014024: D0 76 SE_STW R7,0x0(R6)SPP_MCM.EEGR.R= 0x0000; 0x00014026: 70 1F E7 F4 E_LIS R0,0xFFF4 0x0001402A: 48 07 SE_LI R7,0x0 0x0001402C: 01 06 SE_MR R6,R0 0x0001402E: 5C E6 00 4A E_STH R7,0x4A(R6)I have a reset on the execution of: 0x00014016: 62 10 SE_BGENI R0,0x1 This is not the behavior I expect, as on the manual is written that ECC is calculated on writings and checked at readings.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.