2020-01-28 9:13 PM
Hi All,
I am unable to connect target to the UDE.
1)Is there any necessity to install virtual Com port drivers for debugging with UDE-STK-PLUS debugger apart from the drivers provided by the UDE software ?
2) How to integrate SPC5 studio with UDE-STK-PLUS ?
3) Also, please share JTAG PIN details of the SPC5-UDESTK-PLUS Debugger. So that I can verify the target connection with UDE-STK-PLUS.
Thanks in advance.
2020-01-30 1:32 AM
Hello Sk ,
1) No, Virtual Com Port drivers are only useful to use Serial Port (using printf mecanism)
2) There are "UDE Eclipse 4 integration" in http://spc5tools.spc5studio.com/
you can install it
but PLS UDE should be installed in your PC
3) Which board do you use ? i think that the information is in the datasheet
Best Regards
Erwan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.