2022-11-23 11:53 PM
On the SPC582B, there is only one SARADC and I would like to reduce the SW time needed for ADC conversion.
I have about 15 ADC to convert and they are not contiguous.
I use the SARADC in scan mode and I would like to retreive my ADC data in a buffer in RAM.
Is it possible to give a list of channels to the DMA when they are not contiguous ?
If not, is it possible to configure several DMA on the same SARADC ?
Is it possible to directly give the buffer adress in RAM to the SARADC?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.