2024-10-07 12:00 AM - last edited on 2025-05-05 11:37 PM by Peter BENSCH
I have successfully established a connection between SPC584B and UDE STK2 as shown below:
In the UDE STK menu, under Config -> Target interface... -> xPC56x/xPC57 Options, when I changed the 256-bit password for Censorship unlocking from the default value to all 0xFF, I was still able to connect via JTAG.
Therefore, I believe that the JTAG password lock is not activated.
According to the RM0449 Reference Manual, it seems that I need to set the DBL bit of LOCK3_PGn to 1 to enable the JTAG password lock.
However, I do not know the address of LOCK3_PGn. Also, how can I modify the DBL bit of LOCK3_PGn?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.