2015-02-17 6:46 AM
I am testing CAN filtering Function on SPC560P,But am not clear about how CAN Mask working.
Configure as following: Rx ID =0, Rx Individual Mask = 0xFFFFFF8; BCC = 1; From my understanding, then the CAN Node can Receive ID from 0 to 7, but cannot , only still can receive ID = 0; stop at BUF00 Rx Flag checked; But , when I set Rx Individual Mask = 0; all CAN ID can be received (stop at BUF00 Rx Flag checked); So, How the CAN ID Mask Working? ----------------- CAN_0.RXIMR[0].R = 0xFFFFFFF8; /*Rx Individual Mask*/ CAN_0.BUF[0].ID.B.STD_ID = 0x0; /*Rx ID = 0*/ /*Check ID Receive*/if(1== CAN_0.IFRL.B.BUF00I){
CAN_0.IFRL.B.BUF00I = 1; // rx completed}
Solved! Go to Solution.
2015-02-24 7:30 AM
Hello Chu ,
Rx ID =0, Rx Individual Mask = 0xFFFFFF8; BCC = 1 Rx Individual Mask is used for acceptance for ID Filtering and the FIFOMask Bits
For normal Rx MBs, the mask bits affect the ID filter programmed on the MB. For the Rx FIFO,the mask bits affect all bits programmed in the filter table (ID, IDE, RTR).0 The corresponding bit in the filter is “don’t care.�?1 The corresponding bit in the filter is checked against the one received. I do not think that for STD_ID=0, RXIMR is useful with mask system you should use a STD_ID different of 0. do you use the interrupt handler to retrieve the CAN Data ?/*
* @brief interrupt handler.
*
* @isr
*/
OSAL_IRQ_HANDLER(vector88) {
OSAL_IRQ_PROLOGUE();
// .. your handler ...
OSAL_IRQ_EPILOGUE();
}
Best regards
Erwan
2015-02-24 7:30 AM
Hello Chu ,
Rx ID =0, Rx Individual Mask = 0xFFFFFF8; BCC = 1 Rx Individual Mask is used for acceptance for ID Filtering and the FIFOMask Bits
For normal Rx MBs, the mask bits affect the ID filter programmed on the MB. For the Rx FIFO,the mask bits affect all bits programmed in the filter table (ID, IDE, RTR).0 The corresponding bit in the filter is “don’t care.�?1 The corresponding bit in the filter is checked against the one received. I do not think that for STD_ID=0, RXIMR is useful with mask system you should use a STD_ID different of 0. do you use the interrupt handler to retrieve the CAN Data ?/*
* @brief interrupt handler.
*
* @isr
*/
OSAL_IRQ_HANDLER(vector88) {
OSAL_IRQ_PROLOGUE();
// .. your handler ...
OSAL_IRQ_EPILOGUE();
}
Best regards
Erwan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.