2020-07-29 1:40 AM
my SPC5studio version is 6.0.0,my UDE STK version is 5.0
Solved! Go to Solution.
2020-08-21 7:18 PM
after few days using SPC5studio,I found that the way to solve this problem may not be change your SPC5studio version,you can check your frequency of External crystal , and check whether or not it is corresponding to the Settings of your SPC5studio!!!!
2020-07-29 2:11 AM
I have see other QAs,but i can not find a proper method for my project
2020-07-29 2:11 AM
2020-07-29 2:12 AM
and my main function is:
/* Inclusion of the main header files of all the imported components in the
order specified in the application wizard. The file is generated
automatically.*/
#include "components.h"
#include "can_lld_cfg.h"
/**
* FLEXCAN Error callback. Interrupt sources managed are: Bus Off, Error, Tx Warning and Rx Warning.
*
* canp Pointer to the @p CAN Driver object triggering the error
* esr ESR Register Value
* rx_err_counter Receive Error Counter
* tx_err_counter Transmit Error Counter
*/
void cfg0_errorcb(CANDriver *canp, uint32_t esr,uint8_t rx_err_counter, uint8_t tx_err_counter){
/* Put error management code Here */
(void)canp;
(void)esr;
(void)rx_err_counter;
(void)tx_err_counter;
}
/**
* FIFO notification callback
*
* canp pointer to the @p CAN Driver object triggering the callback
* crfp RX frame containg data
*/
void cfg0_Fifo_RX(CANDriver *canp, CANRxFrame crfp) {
if (crfp.IDE == CAN_IDE_EXT && crfp.EID == 0x70U) {
// pal_lld_togglepad(PORT_E, PE_LED1);
}
if (crfp.IDE == CAN_IDE_STD && crfp.SID == 0x11U) {
// pal_lld_togglepad(PORT_E, PE_LED2);
}
(void)canp;
}
/*
* Application entry point.
*/
int main(void) {
CANTxFrame txmsg;
CANRxFrame rxmsg;
/* Initialization of all the imported components in the order specified in
the application wizard. The function is generated automatically.*/
componentsInit();
/* Enable Interrupts */
irqIsrEnable();
/*
* Activates the CAN driver 1.
*/
can_lld_start(&CAND1, &can_config_cfg0);
/*
* CAN TX Message structure.
*/
txmsg.IDE = CAN_IDE_EXT;
txmsg.RTR = CAN_RTR_DATA;
txmsg.LENGTH = 8U;
txmsg.data32[0] = 0x55AA55AAU;
txmsg.data32[1] = 0x00000000UL;
/* Application main loop.*/
for ( ; ; ) {
txmsg.data32[1]++;
/* Transmit Can message received by mailbox */
txmsg.IDE = CAN_IDE_EXT;
txmsg.EID = 0x8901234UL;
while (can_lld_transmit(&CAND1, 1, &txmsg) == CAN_MSG_WAIT) {
}
/* Transmit Can message received by FIFO */
txmsg.IDE = CAN_IDE_EXT;
txmsg.EID = 0x70;
while (can_lld_transmit(&CAND1, 2, &txmsg) == CAN_MSG_WAIT) {
}
/* Transmit Can message received by mailbox */
txmsg.IDE = CAN_IDE_STD;
txmsg.SID = 0x11L;
while (can_lld_transmit(&CAND1, 3, &txmsg) == CAN_MSG_WAIT) {
}
/*
* Receives the RX CAN Message.
*/
if (can_lld_receive(&CAND1, 1, &rxmsg) == CAN_MSG_OK) {
// pal_lld_togglepad(PORT_E, PE_LED3);
}
osalThreadDelayMilliseconds(250UL);
}
}
2020-07-29 2:15 AM
i have change the samples code, and i change the platform from SPC560B50L5 to SPC560B50L1,and remove PE_LED1-PE_LED4 in Board Initialization Component. other contents that I have no change.
2020-07-29 2:26 AM
I have test the PIT samples code,but it doesn't work as well.
2020-07-30 5:30 PM
I have already fixed my problem, the reason is my SPC5studio version, I have replaced it with the version which was provided by ST technology support.
2020-08-13 2:17 AM
Hello ,
For this case , it is often a configuration clock issue.
Which Board do you use ?
Best Regards
Erwan
2020-08-21 7:18 PM
after few days using SPC5studio,I found that the way to solve this problem may not be change your SPC5studio version,you can check your frequency of External crystal , and check whether or not it is corresponding to the Settings of your SPC5studio!!!!
2021-07-28 9:06 PM
Hi,
May I ask you more details, how you solved the problem.
I am having exactly the same issue.
My target board is SPC582B60E1 (64 pin)
SPC5studio version is 6.0.0 and my UDE STK version is 5.0
Stuck in SPCSetRunMode() in __early_init()
Please share your experience little more elaborate way.
I have checked External oscillator setting as you mentioned. My external oscillator is 40MHz and SPC5 studio setting also have same value.
Regards
D.Kumar
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.