2015-10-10 12:57 AM
Hi,
I am testing SPC560P50L5 with spc5_studio, the built-in example for FlexCAN is loopback test. When I disable loopback and enable supervisor mode, there is nothing on the CAN_TXD pin. I do not know the problem, and I need your help.Is there any good examples(FlexCAN) for me?thanks.2015-10-12 8:52 AM
Hello Michael ,
the built-in example is using the Loopback mode.if you are not using this loopback mode. Configure correctly your pin (Cf reference Manual)and you have to take care about TX Mailbox , RX Mailbox and your RX ID. Best regards Erwan2015-10-13 12:55 AM
Hi Erwan,
I configured the Flex_CAN0 PIN: TXD(B[0]) and RXD(B[1]), Supervisor mode. MB 8~31 are set to be TX mailbox.But after I set the code field 0xc for transmission once, I read the code field back is still 0xc, and noting on the TXD pin.I need your further help, thanks.The transmission function is as below:canmsg_t can_lld_transmit(CANDriver *canp, canmbx_t mailbox, const CANTxFrame *ctfp) { CAN_TxMailBox_TypeDef *tmbp = NULL; uint8_t mbid = 0; /*check if mailbox is non empty */ if (!can_lld_is_tx_empty(canp,mailbox)){ return CAN_MSG_WAIT; } irqIsrDisable(); /* Pointer to a free transmission mailbox.*/ if (mailbox == CAN_ANY_MAILBOX) {#if SPC5_CAN_USE_FLEXCAN0 if(&CAND1 == canp) { for (mbid = 0; mbid < CAN_TX_MAILBOXES; mbid++) { if ((canp->flexcan->BUF[mbid + CAN_RX_MAILBOXES].CS.B.CODE & 8U) == 1) { tmbp = (CAN_TxMailBox_TypeDef *)&canp->flexcan->BUF[mbid + CAN_RX_MAILBOXES]; break; } } }#endif } else { tmbp = (CAN_TxMailBox_TypeDef *)&canp->flexcan->BUF[mailbox + CAN_RX_MAILBOXES -1]; } /* Preparing the message.*/ if (ctfp->IDE) { tmbp->CS.B.IDE = 1U; tmbp->CS.B.RTR = 0U; tmbp->ID.R = ctfp->EID; } else { tmbp->CS.B.IDE = 0U; tmbp->CS.B.RTR = 0U; tmbp->ID.R = ctfp->SID << 18; } tmbp->CS.B.LENGTH = ctfp->LENGTH; tmbp->DATA[0] = ctfp->data32[0]; tmbp->DATA[1] = ctfp->data32[1]; tmbp->CS.B.SRR = 1; tmbp->CS.B.CODE = 0x0C; irqIsrEnable(); return CAN_MSG_OK;}2015-10-15 8:20 AM
Hello Michael ,
Could you send me your Test application ? Could you confirm me your SPC5Studio version ? you should be on 3.7.0 version. Best Regards ErwanWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.