2021-01-13 6:06 AM
Hi,
In the sample application for SPC584BXXX flash test, the hex file is written on RAM and then executed. I need the hex file to get written on flash and then write some data on other specific sectors of flash. So I modified the linker script by changing the RAM sections by flash at some places but the program doesn't work as expected.
Please help me to get an appropriate solution so that the hex gets written on flash and the FlashWrite Flashinit, FlashErase etc. will work as expected.
Thanks in advance.
Solved! Go to Solution.
2021-02-04 12:51 AM
Hello ,
If you are using SPC5Studio.
Linker file is automatically generated
you have to create a linker file user.ld at the root of the projet (Cf attachement user.log for an example RAM Sections changing)
Best Regards
Erwan
2021-02-04 12:51 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.