cancel
Showing results for 
Search instead for 
Did you mean: 

EV-VN9D30Q100F for SPC582B-DIS or SPC58EC-DIS GUI firmware

PNeub.2
Associate II

Hi,

i need some help for the EV-VN9D30Q100F. It says there is a dedicated Software for the SPC582B-DIS or /EV but i can't find it nowhere. The board connects to the GUI (STSW-EV-M09SPI), so far so good, but without the firmware on the MCU, i can't test the VN9D30.

 

and is there a component in autodevkitstudio for the VN9D30 board ? or will it be released ? i wanted to evaluate the board before i implementing it, into my hardware design ?

1 ACCEPTED SOLUTION

Accepted Solutions
PNeub.2
Associate II

Hey for the community, if someone is having the same problem. I got help from the support, they send me the firmware for the SPC582B-DIS to talk to the SPI-GUI.

 

I hope it will help someone.

View solution in original post

1 REPLY 1
PNeub.2
Associate II

Hey for the community, if someone is having the same problem. I got help from the support, they send me the firmware for the SPC582B-DIS to talk to the SPI-GUI.

 

I hope it will help someone.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.