cancel
Showing results for 
Search instead for 
Did you mean: 

Enabling Serial receive interrupt(UART)

DNewm.1
Associate III

Hello

I'm working with spc560p and I want to enable serial receiv​e interrupt, that whenever data received, it save the data and so on.

I could send data by serial driver as sd_dll_write command and its ok. But when I want to use sd_dll_read, actually mcu stopped. It is cleared that I should use interrupt. But need some help.

Thanks​

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
ODOUV.1
ST Employee

Hello,

happy that it works now.

You must set sync to 0 before each time you call sd_lld_read:

if (sync == 1) {

sync = 0;

sd_lld_read(...);

}

Would you please put a best answer if you are happy of my support.

Best Regards,

-Olivier

View solution in original post

14 REPLIES 14
ODOUV.1
ST Employee

Hello,

you can look at this example "SPC560Bxx_RLA SERIAL DMA Test Application for Discovery"

in low level driver, a RX callback is configured in Low Level Drivers Component->LINFkex Settings->SERIAL configurations

and the configuration structure is given to sd_lld_start in main

Best Regards,

-Olivier

DNewm.1
Associate III

Thanks Olivier :smiling_face_with_smiling_eyes: ​

DNewm.1
Associate III

Hello

I think this interrupt will be enable when the receive was complete. In this case, I can't read my receive buffer. So as the uart protocol is active low, we need interrupt that enable with falling edge.

Would you please interduce me interrupt ​that would be enable with falling edge?

Thanks​

ODOUV.1
ST Employee

Hello,

we have roughly 2 main ways to read on UART driver.

1) In synchronous mode (SerialConfig.api_mode=SPC5_LIN_API_MODE_SYNCHRONOUS)

you call function sd_lld_read(buffer, N) and when it returns, the buffer was fulfilled with N bytes so you can process them.

2) In asynchronous mode (SerialConfig.api_mode=SPC5_LIN_API_MODE_ASYNCHRONOUS)

you configure a callback function in SerialConfig.rx_end_cb = myRXCB;

you reset a global variable sync = 0;

you call function sd_lld_read(buffer, N) and when it returns, the RX process was started but the buffer is empty.

when the buffer will be full with N bytes, your callback function will be called:

void myRXCB(SerialDriver *sdp)

{

sync = 1;

}

after calling sd_lld_read, you must wait your buffer is full before to process it:

while(sync == 0);

Best regards,

-Olivier

DNewm.1
Associate III

Hello Olivier

Thanks for your attention and answering. I enabled myRXCB and wrote below code:

void myRXCB(SerialDriver *sdp)

{

(void​)sdp;

sync = 1;

​while(sync ==1){

pal_togglepad(portD, pad7); ​

}

}

Or​

void myRXCB(SerialDriver *sdp)​

{

​(void​)sdp;​

sync = 1;​

​while(sync ==1){

sd_lld_write(&SD1, 0xAA, 1); ​​

}​

}

​and I have another mcu as master to send uart code to my spc560.

​But in these two case, nothing happened. No led blinks an no 0xAA.

ODOUV.1
ST Employee

Hello,

I would recommend you to not put too much code in the callback function, because it should return as soon as possible and avoit re-entrance calling UART interface (such as sd_lld_write)

at minimum, do never put a while instruction in the callback because you never know how many time you will spend in.

you could just write it like this:

void myRXCB(SerialDriver *sdp)

{

(void​)sdp;

sync = 1;

pal_togglepad(portD, pad7); ​

}

and register this myRXCB into the structure passed as second parameter of sd_lld_start

be sure that your portD and pad7 are well configured and wired to your LED on your PCB

in order to see the LED toggling, you need to wait at least 200ms between two sd_lld_read in your main program:

  sd_lld_read(&SD1, ... );

   osalThreadDelayMilliseconds(200);

Best regards,

-Olivier

ODOUV.1
ST Employee

Do you use your own PCB ? or do you use one of our Discovery boards ? (SPC56P-Discovery - Discovery Kit for SPC56 P line - with SPC560P50L5 MCU - STMicroelectronics)

Hello,

Thanks for your answering, I tried this method and it works correctly:thumbs_up:. But callback function works once so when sync rest to zero after all, it doesn't work again and callback didn't work as sync = 1 .

So how should it works again an callback put 1 in sync again too?

My code:

​void myRXCB(SerialDriver *sdp)

{

(void​)sdp;

sync = 1;

}

.

.

.

for(; ;){

if(sync == 1){

​sd_lld_read(&SD1, buffer,1);

​if(buffer ==0xAA){

pal_togglepad(portD, pad7);

}​

sync=0;

}

else{

sync=0;

}

}​

Hello,​

I use my own PCB​.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.