2019-10-20 12:55 AM
Hi all,
do you offer a working C Code example to
program a double word in DFLASH.
E.g. of data 0x55AA55AA at address 0x00AAA8 and data 0xAA55AA55 at address 0x00AAAC?
The example in the RM0037 Reference manual is no C Code
and the EEPROM Emulator (SPC5Studio) is also not written in C Code.
RM0037 Reference manual
Example 10
Double word program of data 0x55AA55AA at address 0x00AAA8 and data
0xAA55AA55 at address 0x00AAAC
MCR= 0x00000010;/* Set PGM in MCR: Select Operation */
(0x00AAA8)= 0x55AA55AA;/* Latch Address and 32 LSB data */
(0x00AAAC)= 0xAA55AA55;/* Latch 32 MSB data */
MCR = 0x00000011;/* Set EHV in MCR: Operation Start */
do /* Loop to wait for DONE=1 */
{ tmp = MCR;
/* Read MCR */
} while ( !(tmp & 0x00000400) );
status= MCR & 0x00000200;/* Check PEG flag */
30.6.3
MCR = 0x00000010;/* Reset EHV in MCR: Operation End */
MCR = 0x00000000;/* Reset PGM in MCR: Deselect Operation */
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.