2014-09-03 7:46 AM
Hello,
on SPC56EL60, I'm using an external 16MHz XTAL so I changed the ''XOSC Clock'' value in the configuration (default is 40MHz). I'm getting the error: ''SPC5_FMPLL0_VCO_CLK outside acceptable range (SPC5_FMPLLVCO_MIN...SPC5_FMPLLVCO_MAX)'' To solve this I have to modify SPC5_FMPLL0_IDF_VALUE and SPC5_FMPLL0_NDIV_VALUE value's that are used to calculate SPC5_FMPLL0_VCO_CLK. These defines are code generated and I can't find them in the application config. Can you please explain how the setup the clock peripheral and keep the overide values unchanged while regenerating code? Thank you2014-09-05 1:33 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.