Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

How do you set CAN Filter to allow only exact CAN IDs?

I am trying to set the CAN bus rx filter so that only the CAN message IDs that I specify in the can_lld_cfg.c file will be received. I tried to use the CAN classic filter setup for extended IDs. I set the mask to all ones (0x0fFFFFFFUL) so, it should...

SLam.1 by Associate
  • 1754 Views
  • 0 replies
  • 0 kudos

SPC560 Series, Ask about data write lock

In the spc 560 series, the data written to Data Flash Array 0 is not replaced with the tool I have. Which register value should I change? Or is there another way?

용이.1 by Associate
  • 918 Views
  • 0 replies
  • 0 kudos

EIRQ

hI, can someone explain this line for me?what mean by  IRQ_PROLOGUE(); EPILOGUE AND DISRO.0 ?] 

0693W00000QKdM5QAL.png
Angle by Associate II
  • 1914 Views
  • 4 replies
  • 0 kudos

In SPC560P44L3 - NMI Interrupt loation

Hi STMCurrently am using SPC560P44L3 , the usage is need to wake up the system when IGNITION is ON.Guide me how to use NMI and where to write the interrupt program. Interrupt vector address location needed to write the program.Thanks and RegardsThila...

ThilakS by Associate II
  • 850 Views
  • 0 replies
  • 0 kudos