Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC5 Studio Download Issue(Evaluation)

Posted on November 19, 2014 at 15:34Hy,     I am trying to request for the evaluation version of SPC5 Studio but the request immediatly rejected i dont know the reason.Is there any evaluation version or student version??Kindly guide me 

sanwal by Associate II
  • 2109 Views
  • 5 replies
  • 0 kudos

SPC5STudio 3.3.0 is available !

Posted on November 07, 2014 at 15:07Dear Users, The 3.3.0 release is now available on the update site. Main improvements: - Patch mode of generated components: You can now modify the generated source code, and keep your modifications even if regener...

SPC560D clock source

Posted on October 08, 2014 at 15:56Hello, If I am using the command ''asm volatile (''nop'');'', how long should the controller need to execute this command? I ask this question because I have tried to use it as an indicator for the system clock. ...

Patriks by Senior
  • 1002 Views
  • 1 replies
  • 0 kudos

Resolved! SPC560D UART

Posted on October 16, 2014 at 12:24Hello, I have some problems understanding and using the UART HAL component.   The test application for the SPC560D sends ''Hello World'' with the chnWriteTimout() function. To send the value 0x55, I wrotechnWriteTi...

Patriks by Senior
  • 2437 Views
  • 4 replies
  • 0 kudos

Can't compile on Windows 8.1

Posted on November 03, 2014 at 19:16I have clear Windows 8.1 (just restored from rescue disks) on Lenovo T540p notebook. I setup latest version of spc5 studio. When I try to compile sample I get error messages. I mark with bold text error. Under Win...

vromanov by Associate II
  • 1471 Views
  • 2 replies
  • 0 kudos

BUG: Pin 144 not exist in PinMap editor for LQFP144 package

Posted on November 03, 2014 at 23:17How to reproduce 1) Open Spc5studio 2) Create test application for SPC56xL Discovery 3) Open PinMap Wizard 4) You can see pins 1-143. Pin 144 not exist Also image not match to image on  SPC56EL70L5 documentation. ...

vromanov by Associate II
  • 1970 Views
  • 3 replies
  • 0 kudos

Unable to start SPC5 studio after crash

Posted on October 21, 2014 at 14:05Hello, I am not able to start SPC5 Studio after it crashes during I worked with the pin map wizard. When I start the application, it only shows me that an error log in the .log has been created. The entry shows me ...

Patriks by Senior
  • 2302 Views
  • 6 replies
  • 0 kudos

out.elf: cannot generate out.elf - Build command doesn't work.

Posted on September 30, 2014 at 14:45Hello, I installed SPC5Studio 3.0.0, and UDE 4.02.05. When i build a new project clicking on ''build all'' icon, SPC5Studio doesn't generate out.elf file, so i am not able to debug. I can debug Software examples ...

paolo2 by Associate II
  • 4079 Views
  • 11 replies
  • 0 kudos

License Expired

Posted on September 30, 2014 at 12:53Hi, I purchased a full license for 1-year, used it only for three months and today the error message came up as follow: main.c:1:0: internal compiler error: initialising license system Demo license has expired (-...

bycc by Associate
  • 1708 Views
  • 3 replies
  • 0 kudos