2025-11-05 5:18 AM - last edited on 2025-11-05 5:40 AM by Andrew Neil
Moved from STM32 forum - this is not an STM32 question.
I am facing an issue with the Auto Dev Kit debugger. My previous license had expired (Hightec), and although I tried renewing it and even registered to get a new license, the debugger still does not work.
Additionally, I notice that the debugger and flash icons appear greyed out.
Could you please assist me in resolving this issue?
Solved! Go to Solution.
2025-11-10 7:07 AM
I have solved the issue, autodevkit works with free license and the error at the start confuses you with pro that you think is not installed, but actually its the free complier which is working. So to conclude we can can just ignore the pro compiler error.
2025-11-05 5:25 AM
> My previous license had expired (Hightec), and although I tried renewing it and even registered to get a new license, the debugger still does not work.
This debugger licence management is fully in the hands of Hightec, nobody on this MCU forum can help with that.
They surely have a forum, helpdesk and support team as well.
2025-11-05 5:26 AM
Ok, but also I didn't get the answer for my 2nd question
(Additionally, I notice that the debugger and flash icons appear greyed out.)
Could you please assist me in resolving this issue?
2025-11-05 5:42 AM
As you don't have a licence for the debugger, it doesn't seem unreasonable that its icons are greyed-out.
2025-11-05 5:43 AM
But I'm using the UDE starter kit
2025-11-05 5:48 AM
Right, I thought that was self-explanatory.
> Could you please assist me in resolving this issue?
If you lack the experience to deal with this issue, ask your direct supervisor for assistance.
2025-11-05 5:48 AM
What programmer are you using? which board are you using?
2025-11-05 5:50 AM
I'm using this board AEK-MCU-C4MLIT1
2025-11-05 5:57 AM
Then the UDE debugger is on board up to 256KB of code.
Just open .wsx of the project from UDE.
2025-11-05 5:58 AM
Yes, I did that, but it's still greyed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.