cancel
Showing results for 
Search instead for 
Did you mean: 

L99BM114: Wiring clarification for Unmounted Cells (5S configuration) - Section 6.8

_gabrielfbdiniz_
Associate II

Hello everyone,

We are currently designing a decentralized Battery Management System (BMS) node for our Formula SAE electric car. We selected the L99BM114 due to its robustness in automotive environments and high measurement accuracy.

Our architecture requires this specific node to monitor a 5-series (5S) cell module. Since the L99BM114 supports up to 14 series cells, we will have 9 unused channels.

While reviewing Section 6.8 of the datasheet (Unmounted cells), the exact hardware implementation for our case felt a bit ambiguous. We want to ensure our schematic doesn't trigger false internal diagnostics, such as Cell Open Wire or Balancing Short/Open.

Could anyone clarify the recommended wiring for the unused pins in a 5S configuration? Specifically:

  1. Voltage Sense Pins (C6 to C14): Should all these unused inputs be shorted together and tied to the highest active potential (C5)?

  2. Balancing Pins (S and B) & Filtering: How exactly should we handle the external filtering resistors (RLPF) and the S/B balancing pins for these 9 unused channels? Should they be left floating, or is there a specific pull-up/pull-down tie-off required?

If there is any reference schematic or application note that covers a reduced cell count configuration for this IC, that would be incredibly helpful.

Thanks in advance for the support!

10 REPLIES 10

You asked the same question in a new thread.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.