2022-06-28 5:09 AM
I have q question about TS393 comparator.
Datasheet says :
Wide single supply range 2.7 V to 16 V or dual supplies (±1.35 V to ±8 V)
I dont understand dual supplies condition.What does mean "dual supplies (±1.35 V to ±8 V)"?
Solved! Go to Solution.
2022-06-28 9:06 AM
Welcome, @jsmit.1, to the community!
The TS393 has two pins for the power supply: VCC- (pin 4) and Vcc+ (pin 8), but no pin for GND. The voltage difference between these two pins may be between Vmax=2.7-16V, whereby it doesn't matter whether you connect
You can only process signals that lie in the respective voltage range, i.e. approx. 0...Vmax for unipolar supply and -Vmax/2...+Vmax/2 for bipolar supply.
Does it answer your question?
Regards
/Peter
2022-06-28 9:06 AM
Welcome, @jsmit.1, to the community!
The TS393 has two pins for the power supply: VCC- (pin 4) and Vcc+ (pin 8), but no pin for GND. The voltage difference between these two pins may be between Vmax=2.7-16V, whereby it doesn't matter whether you connect
You can only process signals that lie in the respective voltage range, i.e. approx. 0...Vmax for unipolar supply and -Vmax/2...+Vmax/2 for bipolar supply.
Does it answer your question?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.