2024-03-19 2:56 AM
Hi,
I was wanting to know that if I only use one channel of the TDA7297, say input 1, but not input 2, how should I handle the unused channel?
Should I just leave the unused input floating, or should I tie it to ground, or tie it to ground via a resistor?
Thanks,
Erik
Solved! Go to Solution.
2024-03-19 3:29 AM
Welcome @bushidov, to the community!
let the 2nd input float and its outputs unconnected. The 2nd input is internally connected to a reference voltage with a pull resistor and ensures a stable state. However, as the corresponding outputs are then at about half VCC, you should not connect them anywhere.
Hope that helps?
Regards
/Peter
2024-03-19 3:29 AM
Welcome @bushidov, to the community!
let the 2nd input float and its outputs unconnected. The 2nd input is internally connected to a reference voltage with a pull resistor and ensures a stable state. However, as the corresponding outputs are then at about half VCC, you should not connect them anywhere.
Hope that helps?
Regards
/Peter
2024-03-19 6:52 AM
That does indeed help. I just didn't want to leave anything floating and then it cause some sort of oscillation. I thought I saw the resistor on the internal document, just wanted to be sure.
Thanks,
Erik
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.