2019-04-09 6:59 AM
I like everything about the TS92X series, I just need to know if there are any issues with operating the TS92X series with dual supplies (+5/-5V).
2019-04-09 7:10 AM
Hello,
Maximum operating Vcc is 12V, so, yes TS922 can operate at +/-5V in dual supply.
Best regards
2019-04-09 7:30 AM
I assume this is the same answer for the TS921 since they are the same series, correct?
2019-04-09 7:33 AM
Sure, this is correct also for TS921.
2019-04-09 7:41 AM
Thank you for the quick responses! Have a great day!
2019-04-09 7:55 AM
Thanks to you ! Sure this is a great circuit, what features are most valuable to you ? Do you use it for a specific application ?
Best regards
Antoine
2019-04-09 8:02 AM
The fact that it's unity gain stable with high output current. I'm using this in a GaN device gate bias network.
2019-04-09 8:08 AM
Thanks for the info !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.