2014-05-05 3:07 PM
TS555CN is a low power version of NE555.
TS555CN is made by STAll Datasheets of TS555CN say ''high output current capability''but there is no max output current given in any DataSheet!is the max output current better than with NE555 ?how much is it ?Is there a package of TS555 that can be cooled?thanksGerald Trost #timer-5552014-05-14 11:55 PM
Hello Gerald,
In the table 2 of TS555 datasheet, it is specified the maximum allowed output current. Here follows the maximum output current : Isink (current going into the IC) = 10mA Isource (current going out of the IC) = 50mA In addition, we can note that in the NE555 datasheet, the output current is higher : Isink = 200mA Isource = 200mA Thus, the NE555 has more output current capabilities than the TS555. However, the TS555 has a better current consumption and lower threshold/trigger currents. Regarding your last question, we do not propose this kind of package, but this DIP8 package allows it have a better power dissipation even with a single layer PCB. Please, note also that both TS555 and NE555 are in NRND status (Not Recommended for New Design). Best regards, Sylvain2014-05-15 12:51 PM
Hello Silvian!
Many thanks for the good information.Maybe you also know a stronger ''555'',maybe there is a 555 available with very lowPower consumption like TS555 and highsink-source current of 300mA.If you know this device than please tell me.yours, Gerald2014-05-16 4:02 AM
Hello Gerald,
I'm afraid to tell you that we do not offer timer with such a low current consumption and high output capabilities. However, for your designs don't hesitate to think to our wide portfolio of opamps, comparators, analog switches, voltage references, temperature, pressure sensors or microcontroller to develop you application, making STMicroelectronics your one stop shop. Best regards, SylvainWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.